SNVA966 July 2020 – MONTH LP8864-Q1 , LP8864S-Q1 , LP8866-Q1 , LP8866S-Q1
The following faults can potentially be recovered by system brightness derating:
These power-related faults are mostly caused by the marginal behavior of the power related blocks. Derating the brightness will decrease the loading of the power blocks. It might help to recover those faults.
The brightness derating action could be removed after a certain period (for example, first time attempt after 1 minute, another attempt after 5 minutes). If no fault after brightness derating action is removed, the system could return to normal.