SNVAA80 July   2024 LM5177

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Reverse Current Operation
  6. 3Design Considerations
  7. 4Pin Configurations
    1. 4.1 Other Pin Configurations
      1. 4.1.1 MODE Pin
      2. 4.1.2 IMONOUT
  8. 5Application Measurements
  9. 6Summary
  10. 7References

IMONOUT

The IMONOUT pin have two functions in reverse current operation. The first function is that the pin can be used to monitor the reverse current value when the average current limit feature is not enabled. In this case, a pulldown resistor is needed between IMONOUT pin and GND. The second function is that this pin is also used to provide a compensation to an average current limit loop to limit the reverse current. In this case, a compensation network is required at IMONOUT pin.