Follow the steps below for
TPS389006Q1EVM hardware setup:
- Connect VAUX (J1) and VDD (J2) to 3.3 V
from the power supply.
- Connect GND (J3) to ground from the power
supply.
- Make sure the jumpers are connected as
per the guidelines in the Table 3-2.
- Before allowing the output of the power
supply to be engaged, check if the power supply voltage is set at
3.3 V and the power supply output current is limited to 10
mA.
- Connect the TI's USB Interface Adapter to
J18 (USB2GPIO Connector) using a 10-pin ribbon cable.
- Connect the TI's USB Interface Adapter to
the computer's USB port.
- Connect any voltage supply rail that
needs monitoring to any of the voltage monitoring inputs (MON1 - MON8).
- The description of the TPS389006Q1EVM
connections can be found in Figure 4-1.