Please follow the steps below precisely to
quickly evaluate the TPS389006-Q1. In this quick start, the TPS389006Q1EVM is set up to
monitor several power supply rails after the ACT pin is triggered.
- Make the hardware connections and
software installation described in Section 4.1 have been completed. Feel free to skip the GUI installation if the Fusion Digital
Power Designer for TPS389006Q1EVM GUI has been installed already.
- Power the EVM by turning on the power
supply. Note that the voltage and current limits at the power supply is set at 3.3 V and
10 mA.
- Once the TI's USB Interface Adapter is
connected to EVM and the laptop, launch the evaluation software Fusion Digital Power
Designer.
- Click on I2C GUI on the bottom
right of GUI.
- Click on
Change Scan Mode to select TPS389xxx and then click OK.
- Scan for the
TPS389006Q1EVM by clicking on Scan for TPS389xxx on top left of the window.
- Once the EVM is discovered, select
Click to Configure.
- Once the
Click to Configure box has been selected, the Fusion Digital Power Device GUI for
the TPS389006-Q1 appears as shown below. The GUI image shows the General Config,
Sequencing, Clear/Reset, Telmetry, and Polling (Plotting the
monitored voltage rails) sub-windows.
- The GUI image below continues to show the
additional sub-windows that are in the GUI for the TPS389006-Q1. The GUI image includes
the Interrupt Enable, Voltage Range and Threshold, Status Registers,
and Polling (plotting the monitored voltage rails) sub-windows.
- The last GUI
image below shows the last five registers in the Status Registers sub-window.