Follow the steps below for TPS389006Q1EVM hardware setup:
- Connect VAUX (J1) and VDD (J2) to 3.3V
from the power supply.
- Connect GND (J3) to ground from the power
supply.
- Make sure the jumpers are connected as
per the guidelines in the Table 3-2.
- Before allowing the output of the power
supply to be engaged, check if the power supply voltage is set at
3.3V and the power supply output current is limited to
10mA.
- Connect the TI's USB2GPIO USB interface adapter to J18 (USB2GPIO connector) using a 10-pin ribbon
cable.
- Connect the TI's USB2GPIO USB interface adapter to the USB port of the computer.
- Connect any voltage supply rail that
needs monitoring to any of the voltage monitoring inputs (MON1 - MON8).
- The description of the TPS389006Q1EVM
connections can be found in Figure 4-1.