SNVU785C February   2022  – August 2024 TPS389006-Q1

 

  1.   1
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Related Documentation
    2. 1.2 TPS389006-Q1 Applications
  4. 2Schematic, Bill of Materials, and Layout
    1. 2.1 TPS389006Q1EVM Schematic
    2. 2.2 TPS389006Q1EVM Bill of Materials
    3. 2.3 Layout and Component Placement
    4. 2.4 Layout
  5. 3EVM Connectors
    1. 3.1 EVM Test Points
    2. 3.2 EVM Jumpers
  6. 4EVM Setup and Operation
    1. 4.1 Setup and GUI Installations
      1. 4.1.1 TPS389006Q1EVM Hardware Setup
      2. 4.1.2 TPS389006Q1EVM Software Setup
    2. 4.2 Quick Start to TPS389006Q1EVM GUI
    3. 4.3 Example Operation of TPS389xxx-Q1
  7. 5Revision History

Quick Start to TPS389006Q1EVM GUI

Please follow the steps below precisely to quickly evaluate the TPS389006-Q1. In this quick start, the TPS389006Q1EVM is set up to monitor several power supply rails after the ACT pin is triggered.

  1. Make the hardware connections and software installation described in Section 4.1 have been completed. Feel free to skip the GUI installation if the Fusion Digital Power Designer for TPS389006Q1EVM GUI has been installed already.
  2. Power the EVM by turning on the power supply. Note that the voltage and current limits at the power supply is set at 3.3V and 10mA.
  3. Once the TI's USB2GPIO USB interface adapter is connected to EVM and the laptop, launch the evaluation software Fusion Digital Power Designer.
  4. Click on I2C GUI on the bottom right of GUI.
    TPS389006Q1EVM Fusion Welcome Window Figure 4-8 Fusion Welcome Window
  5. Click on Change Scan Mode to select TPS389xxx and then click OK.
    TPS389006Q1EVM Fusion Scan Window Figure 4-9 Fusion Scan Window
    TPS389006Q1EVM Fusion Scan Selection
              Window Figure 4-10 Fusion Scan Selection Window
  6. Scan for the TPS389006Q1EVM by clicking on Scan for TPS389xxx on top left of the window.
    TPS389006Q1EVM Fusion Scan Window - Scanning for
              TPS389006Q1EVM Figure 4-11 Fusion Scan Window - Scanning for TPS389006Q1EVM
  7. Once the EVM is discovered, select Click to Configure.
    TPS389006Q1EVM Fusion Scan Window - Scan for
              TPS389006Q1EVM Completed Figure 4-12 Fusion Scan Window - Scan for TPS389006Q1EVM Completed
  8. Once the Click to Configure box has been selected, the Fusion Digital Power Device GUI for the TPS389006-Q1 appears as shown below. The GUI image shows the General Config, Sequencing, Clear/Reset, Telemetry, and Polling (Plotting the monitored voltage rails) sub-windows.
    TPS389006Q1EVM Fusion Digital Power Device GUI -
              TPS389006Q1EVM (Image #1) Figure 4-13 Fusion Digital Power Device GUI - TPS389006Q1EVM (Image #1)
  9. The GUI image below continues to show the additional sub-windows that are in the GUI for the TPS389006-Q1. The GUI image includes the Interrupt Enable, Voltage Range and Threshold, Status Registers, and Polling (plotting the monitored voltage rails) sub-windows.
    TPS389006Q1EVM Fusion Digital Power Device GUI -
              TPS389006Q1EVM (Image #2) Figure 4-14 Fusion Digital Power Device GUI - TPS389006Q1EVM (Image #2)
  10. The last GUI image below shows the last five registers in the Status Registers sub-window.
    TPS389006Q1EVM Fusion Digital Power Device GUI -
              TPS389006Q1EVM (Image #3) Figure 4-15 Fusion Digital Power Device GUI - TPS389006Q1EVM (Image #3)