SNVU797C April 2022 – October 2024 LM5177
These switches enable to set the resistor for the CFG pin. Details can be found in the LM5177 Wide VIN 4 Switch Buck Boost Controller Core IP data sheet.
# | DRSS | SCP – Hiccup Mode | PSM Entry Threshold | Current Limit |
---|---|---|---|---|
1 | DISABLED | DISABLED | 10% | DISABLED |
2 | ENABLED | |||
3 | DISABLED | ENABLED | ||
4 | ENABLED | |||
5 | DISABLED | DISABLED | 10% | ENABLED |
6 | ENABLED | |||
7 | DISABLED | ENABLED | ||
8 | ENABLED | |||
9 | DISABLED | DISABLED | 15% | DISABLED |
10 | ENABLED | |||
11 | DISABLED | ENABLED | ||
12 | ENABLED | |||
13 | DISABLED | DISABLED | 15% | ENABLED |
14 | ENABLED | |||
15 | DISABLED | ENABLED | ||
16 | ENABLED |