SNVU894 December   2024 LM5169

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
    5. 1.5 General TI High Voltage Evaluation User Safety Guidelines
  8. 2Hardware
    1. 2.1 Quick Start Procedure
    2. 2.2 Detailed Descriptions
      1. 2.2.1 Compatibility With the LM5017
  9. 3Implementation Results
    1. 3.1 Performance Curves
    2. 3.2 EVM Characteristics
  10. 4Hardware Design Files
    1. 4.1 Schematic
    2. 4.2 PCB Layout
    3. 4.3 Bill of Materials
  11. 5Additional Information
    1. 5.1 Trademarks

Detailed Descriptions

This section describes the connectors and the test points on the EVM and how to properly connect, set up, and use the LM5169FEVM. See Figure 2-3 for the location of connectors and jumpers.

    VOUTOutput voltage of the converterVOUT screw terminal connector. Apply load to this connector (+ and –). The VOUT test point is used to monitor output voltage.
    VOUT2Secondary output voltage of the converterVOUT2 screw terminal connector. One side of this output is connected to the primary ground (GND) through a tie resistor, Rtie (R12). This resistor can be removed for a true floating voltage source. Apply load to this connector (+ and –).
    GNDGround of the converterGND and GNDS test points. Used as ground test points for the EVM.
    VINInput voltage to the converterVIN screw terminal connector. Apply input voltage to this connector (+ and –). The VIN test point is used to monitor input voltage.
    VINEMIInput voltage to input filter of the converterIf this is desired to use the built-in EMI filter on the EVM, then connect the input supply to the VINEMI screw terminal connector (+ and –).
    Input FilterEMI mitigationAn input EMI filter is provided on the EVM. Note L2 and C18 are not populated and must be installed for the EMI filter to operate. Also, note that the maximum input voltage to the filter is 100VDC.
    EN/UVLO JumperSet EN/UVLO pin optionsUse this jumper to enable and disable the EVM. The resistors connected to this pin set the input UVLO thresholds. Input UVLO thresholds are set to approximately 6V and 5.6V. These levels can be changed by changing the values of R5 and R7. For external control of the device, these resistors must be removed and the control signal applied to the center pin of the header. Note that for accurate shutdown current measurement, these resistors must also be removed and the EN input (center pin) grounded.
    1. Jumper open (default setup): Device starts up and shuts down with UVLO.
    2. Center pin connected to ON: Device starts up and shuts down without UVLO.
    3. Center pin connected to OFF: Device is off.
    PGOODThe PGOOD header used as a test point to monitor the power-good indicator. This flag indicates whether the output voltage has reached the regulation level. PGOOD is an open-drain output that is tied to VOUT through a 100kΩ, resistor R10.
LM5169FEVM LM5169FEVM
                                        Test Setup Figure 2-3 LM5169FEVM Test Setup