SPNA249 june   2023 TMS570LC4357-SEP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2SEE Mechanisms
  6. 3Test Device Information
  7. 4Irradiation Facility and Setup
  8. 5SEL Results
  9. 6Summary
  10.   References

Irradiation Facility and Setup

The heavy ion species used for the SEE studies on this product were provided and delivered by the TAMU Cyclotron Radiation Effects Facility [3] using a superconducting cyclotron and advanced electron cyclotron resonance (ECR) ion source. Ion beams are delivered with high uniformity over a 1-inch diameter, circular cross section area for the in-air station. Uniformity is achieved by means of magnetic defocusing. The intensity of the beam is regulated over a broad range spanning several orders of magnitude. For the bulk of these studies, ion fluxes between 104 and 105 ions/s-cm2 were used to provide heavy ion fluences between 106 and 107 ions/cm2. For these experiments, Silver (47Ag) ions were used. Ion beam uniformity for all tests was in the range of 91% to 98%.