SPRACM3E August   2021  – January 2023 F29H850TU , F29H859TU-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   Using the Fast Serial Interface (FSI) With Multiple Devices in an Application
  2.   Trademarks
  3. 1Introduction to the FSI Module
  4. 2FSI Applications
  5. 3Handshake Mechanism
    1. 3.1 Daisy-Chain Handshake Mechanism
    2. 3.2 Star Handshake Mechanism
  6. 4Sending and Receiving FSI Data Frames
    1. 4.1 FSI Data Frame Configuration APIs
    2. 4.2 Start Transmitting Data Frames
  7. 5Daisy-Chain Topology Tests
    1. 5.1 Two Device FSI Communication
      1. 5.1.1 CPU Control
      2. 5.1.2 DMA Control
      3. 5.1.3 Hardware Control
    2. 5.2 Three Device FSI Communication
      1. 5.2.1 CPU/DMA Control
      2. 5.2.2 Hardware Control
        1. 5.2.2.1 Skew Compensation for Three Device Daisy-Chain System
          1. 5.2.2.1.1 CPU/DMA control
          2. 5.2.2.1.2 Hardware Control
  8. 6Star Topology Tests
  9. 7Event Synchronization Over FSI
    1. 7.1 Introduction
      1. 7.1.1 Requirement of Event Sync for Distributed Systems
      2. 7.1.2 Solution Using FSI Event Sync Mechanism
      3. 7.1.3 Functional Overview of FSI Event Sync Mechanism
    2. 7.2 C2000Ware FSI EPWM Sync Examples
      1. 7.2.1 Location of the C2000Ware Example Project
      2. 7.2.2 Summary of Software Configurations
        1. 7.2.2.1 Lead Device Configuration
        2. 7.2.2.2 Node Device Configuration
      3. 7.2.3 1 Lead and 2 Node F28002x Device Daisy-Chain Tests
        1. 7.2.3.1 Hardware Setup and Configurations
        2. 7.2.3.2 Experimental Results
      4. 7.2.4 1 Lead and 8 Node F28002x Device Daisy-Chain Tests
        1. 7.2.4.1 Hardware Setup and Configurations
        2. 7.2.4.2 Experimental Results
      5. 7.2.5 Theoretical C2000 Uncertainties
    3. 7.3 Additional Tips and Usage of FSI Event Sync
      1. 7.3.1 Running the Example
      2. 7.3.2 Target Configuration File
      3. 7.3.3 Usage of Event Sync for Star Configuration
  10. 8References
  11. 9Revision History

Node Device Configuration

The node devices receive the ping packet and they have to generate the EPWM sync signals after a certain delay depending on the order of device in the node. The delay configuration is done in the fsi_daisy_epwmsync_node.syscfg file provided along with the project. The configuration has to be done using the counter value ‘match’ in the Configurable Logic Block (CLB) under the Counter0 tab as shown in Figure 7-6. FSM block contains the logic to generate the EPWM sync-in signal after the match count delay once it gets the ping packet received signal. The CLB configuration done using the sysconfig file can be seen in the clb.html file under the syscfg tab in the project when the project is built using the CPU1_CLB build configuration as is shown in Figure 7-7.

Figure 7-6 CLB Block Configuration
Figure 7-7 Configured CLB Block

Similar to the lead device, the user can configure the EPWM frequency and duty cycle for the respective node using EPWM_TIMER_TBPRD for frequency, EPWM_CMPA_VALUE for EPWM1A duty cycle and EPWM_CMPB_VALUE for EPWM1B duty cycle.

The CLB configuration differs slightly from F28004x to F28002x. F28004x devices have to route CLBx_OUT to FSITX external trigger connection through the EPWM XBAR while the F28002x devices have been updated to directly connect FSITX external connection to CLBx_OUT. User can refer to the device reference manual which explains the specific information.