SPRACM9B June 2019 – November 2020 TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
By varying the control bandwidth and repeating these tests and noting down the resulting gain cross over frequency and phase margin, a set of plots are obtained for Id loop as shown in Figure 11-10. Two sets of tests are performed, one based on classical current control method, and the other based on FCL. Both these tests were performed using different current regulators. They all gave converging results.
The group of plots at the bottom is obtained for conventional control, and it is obvious that the gain cross over frequency is too low and that as the gain cross over frequency is increased, the phase margin drops a lot faster.
The group of plots at the top is obtained with FCL. The gain cross over frequency is nearly thrice that of the classical method for a given phase margin. And also, as the gain cross over frequency is increased, the relative drop in phase margin is very low compared to the classical method. This effectively means that FCL can provide a higher bandwidth or gain cross over frequency at a higher phase margin.