SPRACN0F October 2021 – March 2023 F29H850TU , F29H859TU-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The inputs of an ADC are typically modeled as a switched capacitor circuit where the hold capacitor inside the ADC, Ch, needs to be charged from an unknown voltage to a value close to the input voltage during the acquisition time. An example, taken from the TMS320F2837xD device, is shown in #T5843526-300.
The required acquisition time for charging Ch is determined by the external impedance of passive components, bandwidth of any buffers or sensors, the internal ADC input parasitics, and the resolution of the ADC.
The system designer can make a variety of trade-offs with respect to external circuit cost and complexity vs settling speed, for example:
With all the above possible trade-offs, it is difficult to select a single acquisition time that is appropriate for all analog inputs in the system. C2000 ADCs allow a separate acquisition window to be selected for each channel, giving the system designer a great deal of flexibility to make whatever speed vs signal conditioning circuit cost vs accuracy trade-offs they would like.
The acquisition window (controlled by the ACQPS field of the ADC SOC configuration register) can also be configured over a wide range of values and with a small step size as shown in Table 2-2.
C2000 MCU | Device SYSCLK | Minimum S+H Time | Maximum S+H Time | S+H Time Configuration Resolution |
---|---|---|---|---|
TMS320F28004x and TMS320F28002x | 100 MHz | 80 ns | 5.1 µs | 10.00 ns |
TMS320F2807x,TMS320F28003x | 120 MHz | 75 ns | 4.3 µs | 8.33 ns |
TMS320F2837xD and TMS320F2837xS | 200 MHz | 75 ns | 2.6 µs | 5.00 ns |
There are a variety of ways to model the ADC input, Texas Instruments offers free tools to help design the ADC input driver circuit as well as instructional videos on proper front end component selection.