SPRACN0F October 2021 – March 2023 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
A digital rotary encoder is a device that converts the position of a shaft to a digital signal. There are two main types of encoders:
C2000 CLB technology enables an integrated solution to interface to the most popular digital rotary position encoders, eliminating the necessity for external field-programmable gate arrays (FPGAs) or application-specific integrated circuits (ASICs). The PositionManager BoosterPackplug-in module is a flexible low voltage platform intended for evaluating various encoder interfaces and designed to work with multiple C2000 LaunchPad development kits such as the LAUNCHXL-F28379D, LAUNCHXL-F280049C, or the LAUNCHXL-F280025C.
Below are examples of encoders that are available for evaluation today as part of the Motor Control SDK software package. Future updates are planned to add examples for both the BiSS-C and EnDAT22 protocols.
The Tamagawa T-Format protocol is a popular digital, bidirectional interface for absolute encoders. The easy-to-use library and example software delivered with TIDM-1011 demonstrates Tamagawa's T-Format standard. In this example, the T-Format absolute encoder interface is integrated into the C2000 using on-chip resources such as the CLB, SPI, and GPIO as shown in #T5843526-237. This TI Design includes the following features:
With the recent C2000 MCUs such as TMS320F2837x and TMS320F28004x, it is possible to implement Fast Current Loop (FCL) algorithms that provide a high current loop bandwidth with the same external hardware as used in classical Field Oriented Control (FOC) methods. TI has developed the FCL algorithm on these MCUs and implemented it on the DesignDRIVE IDDK platform. The T-Format encoder interface has been integrated into an evaluation implementation of FCL algorithms on C2000 devices.
Quick Response Control of PMSM Using Fast Current Loop studies the frequency response analysis of current loops in real time and also verifies the interface logic for the T-format encoder interface implemented in TIDM-1011. The position loop in this example can be closed using a QEP encoder or a T-format encoder and FCL can be implemented in both cases.
Incremental rotary encoders output a pulse train to indicate that the shaft being monitored has moved. The system master typically processes this pulse train to determine information such as speed, distance and position. In the QepDiv implementation, position information is sent from the encoder to the Enhanced Quadrature Encoder Pulse (eQEP) module on a C2000 MCU. In the PulseGen case a custom pulse stream is generated to meet the system needs. The PTO-QepDiv example demonstrates how the CLB can be used to generate a divided pulse stream from these eQEP inputs as shown in #T5843526-239. The divided pulse stream can then be sent to another device in the system. Both the QepDiv and PulseGen examples are documented in the C2000 Position Manager PTO API Reference Guide.