SPRAD70 March 2023 AM2631 , AM2631 , AM2631-Q1 , AM2631-Q1 , AM2632 , AM2632 , AM2632-Q1 , AM2632-Q1 , AM2634 , AM2634 , AM2634-Q1 , AM2634-Q1
The AM263x Control Card Evaluation Module (EVM) has 2x INA226/INA228 (in E1/E2 respectively) current monitors that can be used to evaluate this usage. The two current monitors are used to measure the power on the two voltage rails, 1.2V and 3.3V, respectively.
As an example, consider the monitoring and measurement of power on the 1.2V voltage rail. Follow sections 3.1 and 3.2 if you are using the control card with INA226 or sections 3.3 and 3.4 if it has the INA228.