SPRUHM9H October 2014 – May 2024 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076
Up to twelve independent peripheral signals are multiplexed on a single GPIO-enabled pin in addition to the CPU-controlled I/O capability. Each pin output can be controlled by either a peripheral or one of the two CPU masters.
There are up to 8 possible I/O ports:
Figure 7-1 shows the GPIO logic for a single pin.
The USB PHY pin muxing is not shown in Figure 7-1. For more details on USB pins, see Section 7.5.
There are two key features to note in Figure 7-1. The first is that the input and output paths are entirely separate, connecting only at the pin. The second is that peripheral muxing takes place far from the pin. As a result, for both CPUs and CLAs to read the physical state of the pin independent of CPU mastering and peripheral muxing is possible. Likewise, external interrupts can be generated from peripheral activity. All pin options such as input qualification and open-drain output are valid for all masters and peripherals. However, the peripheral muxing, CPU muxing, and pin options can only be configured by CPU1.
A separate configuration is required for the USB signals. See Section 7.5 for details.