SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
The device takes advantage of the system trace infrastructure to provide visibility to the user regarding EVE VCOP micro-task sequencing. This is supported through a SMSET module instantiated in the EVE subsystem. The VCOP start and done events are handled as generic events and encapsulated in STP messages with an event-ID and local timestamp and exported through the CT_STM module.
The EVE instrumentation scheme allows the user to understand micro-task dependencies, and potential bottlenecks. DMA transfer boundaries are reported as EVE events. Software messages from ARP32 execution can be interleaved with EVE VCOP events.