SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
During the booting procedure, the ROM code reads 512-byte sectors from the NAND device. The reading fails in two cases:
The ROM code uses normal read (command 00h 30h) for reading NAND page data.
Page data can contain errors caused by memory alteration. The ROM code uses an ECC correction algorithm to detect and possibly correct those errors. The default ECC correction applied is BCH 8b/sector using the GPMC and ELM hardware.
For device ID codes D3h, C3h, D5h, C5h, D7h, C7h, DEh, and CEh when the manufacturer code (first ID byte) is 98h, the cell type information is checked in the fourth byte of ID data. If it is equal to 10b, the ECC correction applied is BCH 16b/sector.
The BCH data is automatically calculated by the GPMC on reading each 512-byte sector. The computed ECC is compared against the ECC stored in the spare area for the corresponding page. Depending on the page size, the amount of ECC data bytes stored in the corresponding spare area is different. Figure 32-19 and Figure 32-20 show the mapping of ECC data inside the spare area for 2-KiB page and 4-KiB page devices, respectively. If both ECC data are equal, the read sector function returns the read 512-byte sector without error. Otherwise, the ROM code tries to correct errors in the corresponding sector (this procedure is assisted by the ELM hardware) and returns the data if successful. If errors are uncorrectable, the function returns with FAIL.