SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
The Notify bit is used in conjunction with the Notify interrupts and when the channel has completed the DMA transfer the Notify Interrupt for the list that contains the descriptor will fire. The last Notify bit set for a specific list will be used so only a single Notify should be set in a list.