The VCP modules receive event (VCP1REVT and VCP2REVT) are generated when any of the following conditions appear:
- The traceback unit has written top one fourth and half or bottom one-fourth and half of the output FIFO buffer (see Figure 30-11).
- After the traceback is completed (the whole frame has been decoded).
- VCP_VCPIC5[30] OUTF bit is set to 1 and all decisions have been read to read the output registers.