SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
If any two tasks are small enough to fit in program cache, software uses SDP to fetch the contents of the next tasks into program cache while operating on the current task. If that program cache is direct mapped, extra care must be taken to ensure that any two tasks do not reside in the same modulo-32k range of memory.