SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
The 32-bit source address parameter specifies the starting byte address of the source. For SAM in increment mode, there are no alignment restrictions imposed by EDMA. For SAM in constant addressing mode, it must program the source address to be aligned to a 256-bit aligned address (5 LSBs of address must be 0). If this rule is not observed, the EDMA_TPTC returns an error. Refer to Section 16.2.4.12.3 Error Generation for additional details.