SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
Device Level Ring (DLR) support is enabled by setting the DLR_EN bit in the CPSW_CONTROL register. When enabled, incoming received DLR packets are detected and sent to queue 3 (highest priority) of the egress port(s). If the host port is the egress port for a DLR packet then the packet is sent on the CPDMA Rx channel selected by the P0_DLR_CPDMA_CH field in the P0_CONTROL register. The supervisor node MAC address feature is supported with the dlr_unicast bit in the unicast address table entry. When set, the dlr_unicast bit causes a packet with the matching destination address to be flooded to the vlan_member_list minus the receive port and minus the host port (the port_number field in the unicast address table entry is a don’t care). Matching dlr_unicast packets are flooded regardless of whether the packet is a DLR packet or not. The EN_P0_UNI_FLOOD bit in the ALE_CONTROL register has no effect on DLR unicast packets. Packets are determined to be DLR packets as shown below: