SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
Upon detection of erroneous instruction code, parameter, load/store address, or loop in execution exceeding programmed max iteration count, VCOP signals the error by generating an interrupt and registering the error source in the MMR VCOP_ERROR. Refer to register manual for details.
Upon detection of error, VCOP:
Depending on the EVE-level memory switch setting, VCOP’s access of the data memory space may be deemed invalid by the memory switch. When this happens, the memory switch signals VCOP to enter error handling state, as described above. VCOP does not send an error interrupt, as the memory switch is doing that (for invalid access from VCOP or from other masters).