SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
The MAC generates and appends a 32-bit Ethernet CRC onto the transmitted data, if the transmit packet header PASS_CRC bit is 0. For the CPMAC_SL generated CRC case, a CRC at the end of the input packet data is not allowed.
If the header word PASS_CRC bit is set, then the last four bytes of the TX data are transmitted as the frame CRC. The four CRC data bytes should be the last four bytes of the frame and should be included in the packet byte count value. The MAC performs no error checking on the outgoing CRC when the PASS_CRC bit is set.