SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
Different camera sources are interleaved on a line-by-line basis. The beginning of each line carries a Metadata tag that provides key information about that line. This Metadata tag is preceded by a SAV codeword in which F=0, V=0, and H=0.
At the end of the line, an EAV code is inserted with an appropriate number of padding pixels following it. This EAV code has F=0, V=0, and H=1. The startcodes used for the Metadata wrapped lines and the dummy lines form the Super Frame. The VIP_PARSER module has logic to parse out the super frame, analyze the Metadata tags, and frame buffer the line contents appropriately.