SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
The DBP block is used to improve performance for straight line cache misses, by snooping the program cache miss/software preload requests and issuing larger/pipelined burst requests to the system. The DBP block includes a 256-byte buffer that is logically composed of two 128-byte buffers.
When EVE is reset, the buffers are reset to an idle/empty state and DBP defaults to enabled (EVE_BUS_CONFIG[4] DBP_ENABLE = 0x1). When a new cache-line request is detected, the DBP initiates 128-byte burst to the system for the current 128-byte aligned range, and another 128-byte burst for the next 128-byte aligned range. DBP requests never cross the 128-byte boundary. Depending on the alignment of the new cache request, for initial requests with LSB = 0, 128-byte request is issued; for LSB = 0x20, a 96-byte burst is issued; for LSB = 0x40 a 64-byte burst is issued; and for LSB = 0x60, a 32-byte burst is issued. This last case does not allocate space in the prefetch buffer.
Any subsequent cache miss requests that match addresses for the previously prefetched data are returned directly from the prefetch buffer. When a cache request is received for address with LSB = 0x60 (last 32 bytes of a 128-byte aligned buffer), then that 128-byte buffer segment is marked invalid and the next sequential 128 bytes of data is prefetched. The prefetch buffer is always 256 bytes ahead of the program cache miss requests, and operates in ping-pong fashion with each of the 128-bytes buffer segments.
Example:
When a discontinuous cache-line request is received (that is, the request is not allocated [or in flight] in the prefetch buffer), then the entire prefetch buffer is invalidated, and the sequence begins from the start.
The prefetch buffer is invalidated when any user coherence operation is initiated.
DBP is disabled by clearing the EVE_BUS_CONFIG[4] DBP_ENABLE bit. When disabled, all cache miss requests bypass the DBP buffers and are issued to the system as 32-byte demand cache misses.