SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
A VCP modules transmit events (VCP1XEVT and VCP2XEVT) are generated when any of the following conditions appear:
The extra XEVT pulls the next set of input configurations via EDMA. If EDMA controller is not set up to link in another set of input configurations, then a dummy transfer should be set up to avoid an SER Event Flag being set for the EDMA Parameter Entry. If the flag is set, it effectively locks the VCP modules, and must be cleared before any future events can be processed for that entry.