SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
The design supports 64 deep instruction memory. Each of the instructions is 78 bit wide and is stored in a RAM internal to the SPF module. Each instruction can have up to four operands, two arithmetic/logical operations and two conditional jump/save actions based on the outcome of the operations.
The operand field is 52 bits wide and it can have up to four operands. The arithmetic and logical operation codes are four bits each. The operation codes are nine bits each.
Bits | Field Name | Description |
---|---|---|
77:26 | OPERAND | Up to four operands are specified in this field. The source of the operands can be the packet that is being received at the network interface, one of the internal register values or an 8/16/32 bit operand specified within the instruction. |
25:22 | FUNCTION0 | This field specifies a single or dual operand Arithmetic/Logic Function. This function is applied to one or both of first two operands specified in the instruction. |
21:18 | FUNCTION1 | This field also specifies a single or dual operand Arithmetic/Logic Function. This function is applied to one or both of the third and fourth operands specified in the instruction. |
17:9 | OPERATION0 | A Save/Jump/Limit/Nop operation is specified in this function. Save operation code includes the source and destination information. The save source is the output of functions and the destination is one of the internal registers where data should be saved. Jump operation code has information about a condition and a destination. The jump occurs when the condition, which is based on the result of function0 and function1, is true. The Jump destination controls the flow of instruction execution. Jump to location 1 results in the packet being dropped. Rule engine goes back to initial instruction and waits for next packet. The event logger writes information to memory. Jump to location zero results in the packet being accepted. The rule engine goes back to initial instruction and waits for next packet. Limit operation code has information about a condition and a rate limit register. The Limit operation either causes the packet to be dropped or results in the specified rate limit register to be decremented by one. |
8:0 | OPERATION1 | This field specifies a second save/jump operation. The format for this field is same as for Operation0. |