SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
The SATA AHCI engine supports NCQ and is capable of command queued protocol interactions with NCQ-compliant SATA mass storage devices. The NCQ commands generated by a SATA HBA port are loaded into command queues maintained at the peripheral device. The commands are stored in a queue and subsequently fetched and processed by peripheral device controller in sequences, which imply more native and highly-optimized for the device order of execution. The synchronization between an NCQ-aware SATA HBA and an NCQ-aware peripheral storage device involves implementation of the so called FPDMA queued command protocol, which ensures that HBA posts NCQ commands to the target SATA device in its demanded NCQ order.