SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
There are three counters which are used to count different types of errors occured when the ECC mode is enabled. The counters are the following:
When a single error in the 128-bit data word occurs and this error is corrected, the OCM controller indicates for the corrected bit of this 128-bit word by setting to 0x1 a corresponding bit in the corrected bit distribution register. This is a 128-bit register composed by the following registers:
When a single error in the ECC itself occurs, the OCM controller indicates for this error by setting to 0x1 a corresponding bit in the STATUS_SEC_ERROR_DISTR_4[7:0] SEC_ECC_CODE_ERROR_FOUND bit field. The parity bit is not associated with this bit field.