SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
The Subsystem Counter Timer Module (SCTM) is a generic profile counter and timer module that provides the following functions:
The SCTM has eight counters (two of which have timer functions). There are input events going into the SCTM and interrupt events going to the IPU INTC. For more information about the counter configuration and the SCTM input events, see IPU Subsystem Performance Monitoring, in On-Chip Debug Support. For more information about the mapping of the SCTM interrupt event signals to IPU INTC inputs, see Interrupt Requests to IPU1_Cx_INTC, in Interrupt Controllers.
Figure 7-8 shows the SCTM block diagram.