A chained DMA transfer can be programmed as follows:
- Configure the transfer parameters for each logical DMA channel in the chain as in step 1 for either the synchronized or non-synchronized transfers described in Section 18.1.5.5, Concurrent Software and Hardware Synchronization.
- For each channel in the chain, configure the DMA4_CLNK_CTRLi register as follows:
- Next logical DMA channel number (for a looping chained transfer link last channel to first channel number), in the DMA4_CLNK_CTRLi[4:0] NEXTLCH_ID bit field.
- Include the logical channel to the chain and enable link by setting the DMA4_CLNK_CTRLi[15] ENABLE_LNK bit.
- For a non-looping chain, the last logical channel in the chain must have the DMA4_CLNK_CTRLi[15] ENABLE_LNK bit set to 0 to indicate the end of the chain.
- Enable the transfer through the enable bit in the first logical channel DMA4_CCRi[7] ENABLE bit. All other channels in the chain must be disabled. Each channel is enabled automatically in turn when the previous logical channel transfer completes. A non-synchronized transfer starts immediately; a hardware-synchronized transfer starts when the DMA request line corresponding to the first DMA channel in the chain is asserted.
To stop a looping chained transfer, disable the DMA4_CLNK_CTRLi[15] ENABLE_LNK bit (by setting it to 0x0), of the final channel transfer.
In the RAM-to-RAM copy example, to copy in loop, it is possible to link channel 10 on itself. The following line can be added in the channel configuration:
/* g) Set link for loop */
DMA4_CLINK_CTRL_CH10 =
0x0000800A;