SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
The memory spaces cached in ARP32 program cache are not always coherent with the external memory. For example, if the copy of the code in external memory is modified, it is possible that the copy of the code that is cached in L1P is out of date with respect to the corresponding location contents in system memory. This may happen, for example, if software is implemented using code overlays. The application controlling such paging should take the appropriate steps to invalidate a cache that is rendered incoherent.
In addition, the ARP32 breakpoint methodology involves emulation and debug software inserting a breakpoint instruction in the program image in system memory (by replacing a valid instruction). Thus, there is a mechanism to update the cache to reflect the newly inserted breakpoint instruction. This is accomplished with the same software or hardware mechanism.
To allow for such software-directed invalidate, the cache controller supports three methods to invalidate the content of the cache: