SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
A feature was defined for the case of single stream (either discrete sync or embedded sync) input handling where VIP_PORT_A[8] ENABLE for Port A and VIP_PORT_B[8] ENABLE for Port B is taken inactive. The single stream case was deemed more important than the multi-stream one since the output of the VIP_PARSER may be used to drive the Scaler module. The Scaler needs to work on a frame boundary (startframe to endframe) or it may lock up without a reset. The goal of the disable handling for the single stream case is to complete a field or frame of output data to the downstream module. Then, upon enabling of the port again, the system should start up properly without a need to reset the individual modules within the VIP instance.
In this scenario, suppose the VIP_PARSER has been processing a single input stream. Then, ENABLE is brought inactive. The VIP_PARSER will continue to output data downstream until it sends out an endframe pixel and the downstream module accepts the endframe pixel.