SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
Level 1 memory (L1) is split into separate program memory (L1P memory) and data memory (L1D memory). Each of the memories can be split into static RAM (normal addressable on-chip memory) and cache.
L1P memory is dedicated to TMS320C66x CPU program words storage and is interfaced via a dedicated L1P memory controller in the DSP C66x CorePac. User can choose to initialize one part of the L1P memory as cache and the other as SRAM. The entire 32 KiB memory is cacheable. The L1P features a dynamically configurable cache size (4 KiB, 8 KiB, 16 KiB and 32 KiB) defined via L1P controller configuration register - L1PCFG[2:0] L1PMODE bitfield. Note that, the L1P controller maps the cache space by starting at the top of the L1P memory map (i.e. from most significant address) and working downwards. The L1P mapped SRAM size is 32 KiB minus the configured cache size.
The L1P cache / SRAM is ONLY read-accessible by the C66x CPU processor. The DSP C66x CorePac external DMAs (SDMA and EDMA) and internal DMA (IDMA) are the only initiators which can write to the L1P memory. The CPU may however write access and modify certain L1P cache/SRAM controller registers if such access is allowed for the register.
In the device integrated DSP, at reset, the entire 32 KiB- L1P memory is initialized as a cache (reset value of L1PMODE=0x7).
For more information on the L1P cache/SRAM memories, refer to the TMS320C66x DSP Cache User Guide, ( SPRUGY8).
L1D memory is used for level 1 CPU data storage and is interfaced via a dedicated L1D memory controller in the DSP C66x CorePac. User can choose to initialize one part of the L1D memory as cache and the other as SRAM. The entire 32 KiB memory is cacheable. The L1D features a dynamically configurable cache size (4 KiB, 8 KiB, 16 KiB and 32 KiB) defined via L1D configuration register - L1DCFG[2:0] L1DMODE bitfield. Note that, the L1D controller maps the cache space by starting at the top of the L1D memory map (i.e. from most significant address) and working downwards. The L1D mapped SRAM size is 32 KiB minus the configured cache size.
In the device integrated DSP, at reset, the entire 32 KiB- L1D memory is initialized as a cache ( i.e. reset value of L1DMODE = 0x7).
For more information on the L1D cache/SRAM memories, refer to the TMS320C66x DSP Cache User Guide, ( SPRUGY8).