SPRUIE9D May 2017 – May 2024 DRA74P , DRA75P , DRA76P , DRA77P
This event is registered if an error is generated on the interface. The following conditions can cause this:
This is a fatal error in which the DMA is in an error state until software clears the SATA_PxCMD[0] ST bit or resets the interface with a port or global reset. For more information about software-initiated resets, see Section 26.8.4.3.2, Software Initiated Resets.