SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
FILE: fsi_ex1_loopback_cpucontrol.c
Example sets up infinite data frame transfers where trigger happens through CPU. Automatic(Hw triggered) Ping frame transmission is also setup along with data.
User can edit some of configuration parameters as per usecase. These are as below. Default values can be referred in code where these globals are defined
External Connections
For FSI internal loopback (EXTERNAL_FSI_ENABLE == 0), no external connections needed
For FSI external loopback (EXTERNAL_FSI_ENABLE == 1), external connections are required. The FSI TX pins should be connected to the FSI RX pins of the same device. See below for external connections to include and GPIOs used:
External Connections Required between FSI TX and RX of the same device:
GPIO_27 -> FSITXA_CLK
Watch Variables