SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
FILE: mcan_ex1_loopback.c
This example demonstrates Loopback functionality of the MCAN (CAN FD) module. The internal loopback mode is chosen. The transmitted message will be received by the node. All action is internal to the device, hence transmission will not be visible on the MCAN_TX pin. Uses the last address of memory for Rx buffer.
Before running this example, please run the mcan_config_c28x example It will initialize the clock, configure the GPIOs.
External Connections
Watch Variables