SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
FILE: ethernet_ipc_ex1_basic_c28x1.c
This example demonstrates how to configure IPC and pass information from C28x to CM core without message queues. This configures the Pinmux for Ethernet Prepares the Ethernet frame that is sent to the CM core over IPC Message RAM. Uses the IPC command interface to signal the IPC Command, Packet address, Packet Length which is used by CM side code to send it on the Ethernet Line, which is acknowledged by the CM core side code over IPC on succesfully receiving a packet It is recommended to run the C28x1 core first, followed by the CM core.
External Connections
Watch Variables