SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
FILE: ethernet_ex9_revmii_example_revmii_side.c
This example demonstrates the steps to be followed in using the Ethernet of the Communication Manager Subsystem to initialize the Ethernet module and Configure the module in RevMII mode. Before running this Communication Manager code the C28x cpu1 code has to be run to configure the clocks to Communication manager and required IO pads for Ethernet module This Example has been validated on an TI internal board and will not run on Control Card. This has been run with RevMII Example Remote MAC side. Once the RevMII mode is configured this appears like a PHY to the external MAC which is connected over MDIO. Even though there is no physical PHY the RevMII mode lets the remote MAC see this side as a PHY.
External Connections
TBD
Watch Variables