SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
FILE: memcfg_ex2_ram_sysconfig_cpu2.c
This example shows how to assign shared RAM for use by both the CPU2 and CPU1 core. Shared RAM regions are defined in both the CPU2 and CPU1 linker files. In this example GS0 and GS14 are assigned to/owned by CPU2. The remaining shared RAM regions are owned by CPU1.
In this example, a pattern is written to cpu1RWArray and then an IPC flag is sent to notify CPU2 that data is ready to be read. CPU2 then reads the data from cpu2RArray and writes a modified pattern to cpu2RWArray. Once CPU2 acknowledges the IPC flag, CPU1 reads the data from cpu1RArray and compares with expected result.
A timer ISR is also serviced in both CPUs. The ISRs are copied into the shared RAM region owned by the respective CPUs. Each ISR toggles a GPIO. Watch the GPIOs on an oscilloscope, or if using the controlCARD, watch LED1 and LED2 blink at different rates.
Following are the memory allocation details of CPU Timer interrupt ISRs & read(R)/read write(RW) arrays in CPU1 & CPU2 as configured in the example.