SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The CAN module provides several test modes that are mainly intended for self-test purposes. Figure 30-3 aids in understanding the various test modes. Figure 30-3 must be viewed as representative of the module behavior, and not as a gate-accurate implementation of the module. Figure 30-3 does not include the GPIO muxing or the I/O buffers.
For all test modes, the Test bit in the CAN control register needs to be set to 1 to enable write access to the CAN_TEST register.