SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The needs of the application are what ultimately determine the clock configuration. Specific concerns such as application performance, power consumption, total system cost, and EMC are beyond the scope of this document, but must provide answers to the following questions:
If CAN or USB is required, an external clock source with a precise frequency must be used as a reference clock. Otherwise, use only INTOSC2 and avoid the need for more external components.
All of the clocks in the device are derived from one of four clock sources.