SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
In addition to the default interfaces defined in the IEEE 802.3 specifications, the Ethernet module supports several industry standard interfaces to the PHY. The Ethernet module is compliant with the following standards:
The EBC unit has the following capabilities: