SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The read format for a Receive Normal descriptor is made up of a header or Buffer 1 address, reserved field, payload or Buffer 2 or Next Descriptor address, a 30-bit reserved filed, OWN bit, and an interrupt bit.
Figure 43-24 shows the Read Format for a Receive normal descriptor.
In the Receive Descriptor (Read Format), if the Buffer Address field is all 0s, Ethernet module does not transfer data to that buffer and skips to the next buffer or next descriptor.