SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
Each SDFM module has four independent filter modules. These filter modules are identical and can be configured independently. Each individual filter module has the following units:
Figure 28-2 shows the SDFM module block diagram. The SDFM port operation is configured and controlled by the registers listed in Section 28.12.
Each filter module shown in Figure 28-3 has a primary (data) filter and a secondary (comparator) filter pair that receives the same bit stream. Except for the input bit stream, both the primary and secondary filter are completely independent of each other. Each of these filter modules can be independently configured. So, in a SDFM module, there is a total of four primary filters and four secondary filters.