SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
On the CM subsystem, access protection to all the RAMs are done via master specific memory protection unit (MPU) and not in the SRAM controller. Each master on the CM subsystem has a dedicated MPU to filter the accesses. For MSG RAMs, in addition to the MPU, there is logic in-built in the controller to prevent accesses such as fetch or write (if not allowed).