SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The Transmit MII Clock can be gated off in the module save the power when the MAC is in Low-Power Idle (LPI) mode. Setting the LPITCSE in MAC_LPI_Control_Status register enables this feature. This is not applicable to the RMII mode, since the Transmit clock is needed for transmitting the LPI Pattern.