SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
The gasket is disabled by default. When disabled (see Enable Register (Base Address + 0x0C)), the gasket operates in bypass mode and just passes all commands, data, and responses through untouched (though the latency is still added and the CID is still remapped so that order can be preserved in the case where the gasket is enabled or disabled with transactions in flight). In Bypass mode, there are no timed out transactions and thus no timeout interrupts. However, if an unexpected response is received, the unexpected response logic will still work as normal (including issuing an interrupt).