SPRUIZ2 july 2023 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The ADC has been enhanced with capability of hardware oversampling and undersampling with the addition of trigger repeater blocks. The PPB block has also been updated with aggregation features in hardware to support data processing for oversampling and undersampling which would otherwise require software running in lengthy repetitive loops. With the hardware implementation, summation, minimum value, maximum value and other data from oversampled conversions or decimated samples are accessible in registers. Global software trigger has also been added and this feature allows all the ADC modules to convert with a single software trigger. For applications that require more ADC channels offered on F28P65x, an external analog multiplexing IC can be incorporated in the design. Depending on the configuration, the external multiplex IC can have multiple inputs that connect to one output that can be hooked up to any of the ADC input channels of F28P65x device. The multiplex control of the external IC is now supported on the F28P65x ADC in register ADCSOCxCTL with CHSEL and EXTCHSEL fields. The ECAP module on F28P65x can now trigger ADC conversions. Consult the F28P65x TRM for details and examples on the new ADC features.